메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is the clock supplied to WDT a clock before or after rewriting FRQCR?

Latest Updated:03/25/2009

Question:

When multiplication ratio of internal PLL circuit is changed, it counts the PLL setting time by on-chip WDT. At this time, is the clock supplied to WDT a clock before rewriting frequency control register (FRQCR) or a clock after rewriting frequency control register (FRQCR)?

Answer:

The clock supplied to WDT when multiplication ratio of internal PLL circuit is changed is the clock after rewriting frequency control register (FRQCR).

The clock supplied to WDT doesn't stop though the inside of the processor stops temporarily when FRQCR is rewritten.

At this time, clock (PΦ) after the setting of FRQCR is changed is supplied to WDT.

Suitable Products
SH7729R
SH7727
SH7720
SH7709S
SH7706
SH7705
  • 이 기사가 도움이 되셨나요?