메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is the replacement from SH7709S to SH7729R possible?

Latest Updated:03/23/2009

Question:

Is the replacement from SH7709S to SH7729R possible?

Answer:

SH7729R is the one that the DSP function is added to SH7709S.

Since SH7729R has upward compatibility over SH7709S, the replacement from SH7709S to SH7729R is not the problem.

However, the power voltage is different in each frequency version of 100MHz/133MHz/167MHz/200MHz, so confirm the same frequency version when you replace it.

Suitable Products
SH7729R
SH7709S
  • 이 기사가 도움이 되셨나요?