메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What DC characteristics to consider in multiplexed with schmitt?

Latest Updated:03/23/2009

Question:

What should we consider about the DC characteristics of the terminal which is multiplexed with the schmitt trigger pin?

Answer:

Answer
Suitable Products
SH7065
SH7058
SH7055
SH7018
SH7011
  • 이 기사가 도움이 되셨나요?