메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What are the points to check if I use SH7727 to display liquid crystal?

Latest Updated:03/24/2009

Question:

I use the SH7727 LCD controller but the display of liquid crystal module is not well.  Could you please tell me the points that I should check?

Answer:

(1) Firstly, please check if the CAS latency value of SDRAM set in the wait control register 2 (WCR2) bit 6 and 5(wait control of area 3 (A3W1 and A3W0)) and the CAS latency value of SDRAM set in the synchronous DRAM mode register (SDMR) are right.

(2) Set the burst length of SDRAM to one(1).

(3) As for drawing operation, the cache off area has to be used. The SH7727 LCD controller only accesses to the SDRAM of area 3 and it does not access to the cache.

(4) The LCDC data width of SH7727 is 16-bit. As for the connection with the liquid crystal module that has 18-bit digital interface (RGB=6:6:6), R is five(5), G is six(6), and B is five(5). R and B need the process such as setting each least significant bit to pull-down or pull-up.

Suitable Products
SH7727
  • 이 기사가 도움이 되셨나요?