메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What do you mean by an error on the edge detection time of IRQ flag?

Latest Updated:03/24/2009

Question:

At the clear conditions of the edge detection time of the IRQ flag in the hardware manual , it is written that "When interrupt exception processing has been executed", but at what point does this occur?

Answer:

Answer
Suitable Products
SH7065
SH7058
SH7055
SH7018
SH7011
  • 이 기사가 도움이 되셨나요?