What is Interrupt Exception Processing Vectors and Priorities Table?
Latest Updated:03/25/2009
Question:
I do not understand the interrupts whose interrupt sources are I/O listed in the Interrupt Exception Processing Vectors and Priorities Table in the section of the interrupt controller of the hardware manual.
Answer:
The interrupts whose interrupt sources are I/O (0EI/MTUP0E/MTU0EI) are used in the Port Output Enable function (POE). These interrupts are generated according to the settings of P0E# to P03# pins or the output state of large-current pins. Please refer to "Port Output Enable (POE)" in the section of the multifunction timer pulse unit (MTU) of the hardware manual for details.
Suitable Products
SH7144, SH7145 |
SH7047, SH7049, SH7105, SH7107, SH7109 |
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108 |
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045 |