메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the recommended PAD diameter?

Latest Updated:09/28/2009

Question:

What is the recommended PAD diameter?

Answer:

Please refer to SH7619 Group Hardware manual's Appendix (C.Package Dimensions).
SH7619 ball pitch is 0.8 mm. So the recommended PAD diameter is showed as 0.35 mm to 0.45 mm.
Suitable Products
SH7619
  • 이 기사가 도움이 되셨나요?