메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What procedure to get the (SDHI) on Section 18 in the hardware manual ?

Latest Updated:09/28/2009

Question:

What procedure does it need to get the SD Host Interface Specification (SDHI) on Section 18 in the hardware manual ?

Answer:

For users of the SDHI on Renesas products such as the SH7671/SH7673 (SH7670 Series), SoC products, etc. , Renesas will confirm whether you have an SD Host/Ancillary Product License Agreement (HALA) with the SD Consortium, and then request an NDA for the disclosure of the SDHI specification for Renesas products. Please contact your Renesas sales agent about the NDA.
Suitable Products
SH7670
  • 이 기사가 도움이 되셨나요?