메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What the VCL pin is used to?

Latest Updated:03/23/2009

Question:

What the VCL pin is used to?

Answer:

VCL pin is the pin for stabilization of LSI’s internal operating voltage.

It is necessary to connect the capacitor for the internal voltage stability with the VCL pin.

Please refer to the hardware manual of each product for the method of connecting the VCL capacitor.

 

Suitable Products
SH7124, SH7125
SH7146, SH7149
SH7083, SH7084, SH7085, SH7086
SH7058
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
  • 이 기사가 도움이 되셨나요?