메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What to set in LCDC as modulation signal toggle line number register?

Latest Updated:03/24/2009

Question:

What should be set in LCDC ac modulation signal toggle line number register (LDACLNR) ?

Answer:

The alternating current signal may be used for the control to prevent
"burn-in" in LCD panel such as STN. The LCDC ac modulation signal toggle
line number register (LDACLNR) is for setting the lines that toggle this
alternating current signal outputted from M/DISP pin.
Suitable Products
SH7727
SH7720