메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What transfer request is the set value of DMAC DMATCR?

Latest Updated:03/23/2009

Question:

Is the set value of DMAC DMATCR the number of transfers for one transfer request or the number of transfer request accepts?

Answer:

Answer
Suitable Products
SH7065
SH7058
SH7055
  • 이 기사가 도움이 되셨나요?