메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

When Receive Descriptor Empty occurs, how to restart Receive?

Latest Updated:09/28/2009

Question:

When Receive Descriptor Empty (RDE=1 in EESR register) occurs, how to restart Receive?

Answer:

Set RACT bit="1" of the Receive Descriptor and then set RR="1" in EDRRR register. Receive will start.
Suitable Products
SH7619