메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Which pins have Weak Keeper Circuit? And can it select Enable/Disable?

Latest Updated:09/28/2009

Question:

Which pins have Weak Keeper Circuit? And can it select Enable/Disable?

Answer:

Please refer Section 19.6 Usage Note in the hardware Manual. You can not select Enable/Disable. The weak keeper circuit is always Enable.
Suitable Products
SH7619
  • 이 기사가 도움이 되셨나요?