메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Which pins should I use referring to the Pin arrangement in manual?

Latest Updated:03/25/2009

Question:

There are multiple pins with the same name when referring to the Pin Arrangement in the hardware manual. What does this mean? Which pins should I use?

Answer:

Answer
Suitable Products
SH7065
SH7058
SH7055
  • 이 기사가 도움이 되셨나요?