메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Which timing will extend if RAS is set up during CAS BFO RAS refreshment?

Latest Updated:03/23/2009

Question:

If RAS assert cycles are set up during CAS BFO RAS refreshment, which timing will be extended?

Answer:

SH7065=>TRrw is extended.

Except the above => the timing of TRc is extended.

Suitable Products
SH7065
  • 이 기사가 도움이 되셨나요?