메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Why cache operate while CPU become shaky if FRQCR changed?

Latest Updated:03/23/2009

Question:

When the setting of the SH7709S/SH7729R/SH7706/SH7727 frequency control register (FRQCR) is changed, the CPU operation becomes unstable. However, it operates normally when the cache is disabled. Is there any reason?

Answer:

Please check the clock ratio settings of CPU clock and bus clock.

When the ratio of CPU clock cycle to bus clock cycle is 1:1, it cannot be accessed to the SDRAM.

When the burst access is generated to the SDRAM under that setting, the interlock works inside the SH and the SH operation could possibly stop.

When the cache is disabled, the burst access to the SDRAM would not be generated so that it seems to be normally operated but the proper operation is not guaranteed.

Therefore, it should not set the ratio of CPU clock to bus clock to 1:1 when the SDRAM is used.

Suitable Products
SH7729R
SH7727
SH7709S
SH7706