메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Explanation of V850 family orderable part numbers

Latest Updated:10/24/2016

Question:

What is the difference between each part number?

Answer:

Please refer to the links in the below table which link to the appropriate page in the "explanation of orderable part numbers" document.

Please note that this table includes products regardless of status (mass production, non-promotion, others).

Suitable Products
V850 family
  • 이 기사가 도움이 되셨나요?