메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can we talk using simulator and what is input data generation method?

Latest Updated:12/01/2011

Question:

How can communication be realized with the simulator? Also, what is the input data generation method?

Answer:

Either create a 01 pattern using the 01 Editor or create an input file by specifying the pin, data, and timing in the input timing chart window.
Download the input file thus created prior to simulation.
For the concrete method, refer to "Input Timing Chart Editor Window" in the Simulation User's Manual.
Other than that, you can create an external part and call the serial pin data input function as a function of that external part.
Suitable Products
  • 이 기사가 도움이 되셨나요?