메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How should the NC pin of Renesas SRAM be connected?

Latest Updated:03/16/2012

Question:

How should the NC pin of Renesas SRAM be connected?

Answer:

NC (Non Connection) pins of Renesas SRAM aren’t connected inside the chip, so it doesn’t matter how you connect them. You can even leave them unconnected.
Suitable Products
CMOS Operational Amplifiers
Bipolar Operational Amplifiers
CMOS comparators
bipolar comparators
Asynchronous SRAM