메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to deal with unused chip and select pin using SRAM?

Latest Updated:03/16/2012

Question:

For SRAM that has two chip select pins, CS1# and CS2, and SRAM is being controlled using one of them, how should the unused chip select pin be dealt with?

Answer:

When not using CS1# pin, please connect CS2 to Vss of SRAM.
When not using CS2, please connect CS1# toVcc of SRAM.

Suitable Products
Bipolar Operational Amplifiers
Asynchronous SRAM