메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to properly execute USB Control transfer with UPD720150 USB host?

Latest Updated:02/01/2009

Question:

When executing USB Control transfer with the Renesas UPD720150 USB host/peripheral controller, are the stages (Setup, Data, and Status) controlled automatically?

Answer:

No, these stages are not controlled by the uPD720150; they must be controlled by software.
See the user's manual relating to control of these stages for details.
Suitable Products
BD/DVD Recorder
Digital Camera