UPD98410: Malfunctions when logical ports not connected to open PHY
Latest Updated:08/01/2005
Question:
For the UPD98410, to what extent do malfunctions occur when logical ports not connected to PHY are open?
Answer:
Malfunctions may occur with one polling operation in the worst case. The extent of malfunctions depends on various factors.
Suitable Products
BD/DVD Recorder |
Digital Camcorder |
Industrial Network |