메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the order of the pause timer value of the UPD98431?

Latest Updated:08/01/2005

Question:

This question regards the PTVR register (pause timer value read register) of the UPD98431. What is the order of the pause timer value?
Also, is the pause timer value of pause frames transmitted from the MAC side the same order?

Answer:

The pause timer counter unit defined in the IEEE standard corresponds to 1 unit of this register. Concretely, it is 512-bit time.
This unit is also applied to the pause timer value set by the MACC3 register.
Suitable Products
Digital AV